2017-09-26 3:09 AM
I am doing a program where I have a 50Hz square signal and a PWM to generate a sinusoidal with 90 points. Each time
the signal edge of 50Hz is raised or lowered, the timer must be reset and start a new modulation. However, the first two values do not match the programmed width.
void EXTI15_10_IRQHandler(void)
{
//PB10 50H+input float int
//PB11 50H-input float int
if(EXTI_GetITStatus(EXTI_Line10) != RESET)
{
if(MAR==1){
//port_set(PORT_B, 15, 1); //MAR ON
port_set(PORT_A, 4, 1); //ON 50Hz
//TIM2->CCR1=0;
portsONtimer();
}
EXTI_ClearITPendingBit(EXTI_Line10);
}
if(EXTI_GetITStatus(EXTI_Line11) != RESET)
{
if(MAR==1){
port_set(PORT_A, 4, 0); //OFF 50Hz
portsONtimer();
}
//port_set(PORT_A, 4, 0); //OFF 50Hz
EXTI_ClearITPendingBit(EXTI_Line11);
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
This is the timer controlling the PWM:
void TIM2_IRQHandler(void)
{
//static int indice = 0;
TIM2->SR &= ~(1<<0); // clear UIF flag- bit0
switch(dir){
case 0:
if(indice==89){ //change direction of the table
dir= 1;
}
TIM2->CCR1=frec50[indice]; //Increasing table, 1/4 sine
break;
case 1:
if(indice==89){ //change direction of the table
dir= 0;
stop_timer();
}
TIM2->CCR1=frec50[PWM_ELEMENTS - indice - 1];//Decreasing table, 2/4 sine
break;
}
indice = (indice + 1) % PWM_ELEMENTS;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
And this is the function that starts timer:
void portsONtimer(void){
//GPIOA->CRL = (GPIOA->CRL & 0xFFFFFFF0 | 0x00000003); //PA0.1
//port_set(PORT_A, 0, 0); //S
dir= 0;
indice=0;
TIM_Cmd(TIM2, ENABLE);
//TIM2->CCR1=0;
TIM2->CNT = 0;
GPIOA->CRL = (GPIOA->CRL & 0xFFFFFFF0 | 0x0000000B); //PA0
} �?�?�?�?�?�?�?�?�?�?�?
And the stoptimer:
void stop_timer(void){
TIM2->CCR1=0; //negat
//TIM1->CCR2=0;
TIM_Cmd(TIM2, DISABLE);
port_set(PORT_A, 0, 0); //S
GPIOA->CRL = (GPIOA->CRL & 0xFFFFFFF0 | 0x00000003); //PA0.1
TIM2->CNT = 0;
indice=0;
dir= 0;
TIM2->CCR1=0;
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Any idea?
Thank you very much.
Daniel Prieto
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.