2018-05-18 12:20 AM
Hello ,
I am using TIM6 to generate 1 sec of delay and i am toggling LED gpio in the timer ISR
HCLK is 50MHz , prescalar = 999, and period = 49999
The issue is when i use below macro, i get close to 1sec. shown in the pic below
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
and when the that macro is not used. there is a significant difference . I want to know how exactly that macro is affecting here. i can not able to connect the dots. please help
without above macro output
2018-05-18 1:39 AM
Hi
balckiran
,The voltage scaling allows optimizing the power consumption when the device is clocked below the maximum system frequency.
for more details please refer toPower controller (PWR) chapter , Voltage regulator paragraph in you reference manual and General operating conditions in your datasheet :
STM32F7 datasheet example:
-Nesrine-
2018-05-18 3:57 AM
Very sorry , that doesnt answer my question . I want to know why i see difference in timing when scale 3 is used . Thank you .