cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G-DISCO CubeMX Ethernet buglet

hbarta2
Associate III
Posted on December 12, 2016 at 16:51

CubeMX version 4.18.0 sets the PHY Address Value for the on board PHY (LAN8742A) as 1. This does not work. It cannot even be changed in CubeMX without switching to 'user PHY'. 

In order for the on board Ethernet to work the user can go into stm32f7xx_hal_config.h and change the macro that defines LAN8742A_PHY_ADDRESS to 0.

#stm32cubemx-ethernet #stm32f7-discovery-kit
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
stm32cube-t
ST Employee
Posted on January 02, 2017 at 15:48

Hello,

The Phy address name issue will be fixed in next 4.19 release. To change the Phy address value go to the Parameter Settings tab.

View solution in original post

6 REPLIES 6
Imen.D
ST Employee
Posted on December 13, 2016 at 18:24

Hello

Barta.Hank

‌,

I will report your issue internallyfor checking.

Thank you for highlighting this caseand Sorry for the inconvenience it may bring.

Best Regards

-Imen-

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
hbarta2
Associate III
Posted on December 14, 2016 at 20:02

Thank you. 

Another issue is that the Ethernet interrupt priority is left at 0 which does not work with FreeRTOS.

stm32cube-t
ST Employee
Posted on January 02, 2017 at 15:48

Hello,

The Phy address name issue will be fixed in next 4.19 release. To change the Phy address value go to the Parameter Settings tab.

Posted on March 02, 2017 at 13:39

 ,

 ,

I do have the same issue with the code generated for the stm32F2 device.

Additionally some values are not correct, below is the value we should have (based on the demo for the nucleo 207 board).

/* Section 4: Extended PHY Registers */

 ,

♯ define PHY_SR ((uint16_t)0x1FU) /*!<, PHY status register Offset */

♯ define PHY_SPEED_STATUS ((uint16_t)0x0004U) /*!<, PHY Speed mask */

 ,

♯ define PHY_DUPLEX_STATUS ((uint16_t)0x0010U) /*!<, PHY Duplex mask */

♯ define PHY_ISFR ((uint16_t)0x001DU) /*!<, PHY Interrupt Source Flag register Offset */

 ,

♯ define PHY_ISFR_INT4 ((uint16_t)0x0010U) /*!<, PHY Link down interrupt */
Posted on March 06, 2017 at 16:44

refer to

https://community.st.com/0D50X00009XkiUKSAZ

Posted on April 20, 2017 at 00:09

It's not fixed in 4.20.1