Deinitialize USB_OTG_FS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-02 2:07 AM
Hello!
I use cube usb library for usb_otg_fs mode wit STM32L467. I would like to use DM and DP pins also as GPIO INPUT PULL UP when usb is not used.
After usb connection closed, I do the following:
1) I use functions USBD_Stop and USBD_DeInit
2) Disable usb_otg_fs clock
2) Initialize DM and DP pins as GPIO INPUT PULL UP
But after these operations I cannot see high logic level on these pins. Maybe I didn't clear all necessary registers in usb_otg_fs? How should I properly deinitialize usb interface for using DM and DP pins as gpio?
Thank you
#stm32l4-usb #usbSolved! Go to Solution.
- Labels:
-
STM32L4 series
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-05 1:00 AM
So, if somebody will have such problem, i've managed with it. My method is not pretty cool, but it works. If you want to completely de-initialize usb to use DM and DP pins as gpio or in the other way you want, do the following:
1) USB_OTG_FS->GCCFG = 0x00000000; // Simply disable transciever/receiver option by setting PWRDWN bit to 0
2) USBD_Stop( &USBD_Dev );
3) USBD_DeInit( &USBD_Dev );
Steps 2 and 3 are default from ST usb library
You can also use the following method, but for me it was unnecessary:
1) USB_OTG_FS->GCCFG = 0x00000000; // Simply disable transciever/receiver option by setting PWRDWN bit to 0
2) USB_OTG_FS->GPWRDN = 0x00000010;
3) USB_OTG_FS->GADPCTL = 0x00000000;4) USBD_Stop( &USBD_Dev );
5) USBD_DeInit( &USBD_Dev );
Steps 4 and 5 are default from ST usb library
Steps 2 and 3 simply reset configuration USB registers to default values
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-05 1:00 AM
So, if somebody will have such problem, i've managed with it. My method is not pretty cool, but it works. If you want to completely de-initialize usb to use DM and DP pins as gpio or in the other way you want, do the following:
1) USB_OTG_FS->GCCFG = 0x00000000; // Simply disable transciever/receiver option by setting PWRDWN bit to 0
2) USBD_Stop( &USBD_Dev );
3) USBD_DeInit( &USBD_Dev );
Steps 2 and 3 are default from ST usb library
You can also use the following method, but for me it was unnecessary:
1) USB_OTG_FS->GCCFG = 0x00000000; // Simply disable transciever/receiver option by setting PWRDWN bit to 0
2) USB_OTG_FS->GPWRDN = 0x00000010;
3) USB_OTG_FS->GADPCTL = 0x00000000;4) USBD_Stop( &USBD_Dev );
5) USBD_DeInit( &USBD_Dev );
Steps 4 and 5 are default from ST usb library
Steps 2 and 3 simply reset configuration USB registers to default values