cancel
Showing results for 
Search instead for 
Did you mean: 

DMA doesn't copy data from UART RDR

Hicham Chaabane
Associate III
Posted on March 27, 2018 at 12:55

Hello,

I have ported an exisiting code for a UART peripheral that uses DMA to copy the data from stm32F4 to an stm32L4

When I send a character through the UART bus, and wait for the IDLE line detection interrupt to accure, I got the following :

char received in the RDR (receive data register), but is not copied in the DMA Rx buffer that I defined previous

Here how I setup the UART

_t_DeviceHandle.Instance = USART3;

_t_

Device

Handle.Init.BaudRate = 9600;

_t_

Device

Handle.Init.WordLength = UART_WORDLENGTH_8B;

_t_

Device

Handle.Init.StopBits = UART_STOPBITS_1;

_t_

Device

Handle.Init.Parity = UART_PARITY_NONE;

_t_

Device

Handle.Init.Mode = UART_MODE_TX_RX;

_t_

Device

Handle.Init.HwFlowCtl = UART_HWCONTROL_NONE;// UART_HWCONTROL_RTS_CTS;

_t_

Device

Handle.Init.OverSampling = UART_OVERSAMPLING_16;

_t_

Device

Handle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

_t_

Device

Handle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

if (HAL_UART_Init(&_t_DeviceHandle) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

/* Configure USART interrupt */

HAL_NVIC_SetPriority(USART3_IRQn, 5, 0U);

HAL_NVIC_EnableIRQ(USART3_IRQn);

}

Here is how I setup my DMA

  __HAL_RCC_DMA1_CLK_ENABLE();

_t_DeviceRxDmaStreamHandle.Instance =

DMA1_Channel3

;

_t_

Device

RxDmaStreamHandle.Init.Direction = DMA_PERIPH_TO_MEMORY;

_t_

Device

RxDmaStreamHandle.Init.PeriphInc = DMA_PINC_DISABLE;

_t_

Device

RxDmaStreamHandle.Init.MemInc = DMA_MINC_ENABLE;

_t_

Device

RxDmaStreamHandle.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;

_t_

Device

RxDmaStreamHandle.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;

_t_

Device

RxDmaStreamHandle.Init.Mode = DMA_NORMAL; 

_t_

Device

RxDmaStreamHandle.Init.Priority = DMA_PRIORITY_HIGH;

if(HAL_DMA_Init(&_t_

Device

RxDmaStreamHandle) != HAL_OK)

{

assert_failed((uint8_t*)__FILE__, __LINE__);

}

// linking DMA channel with the UART RX

  __HAL_LINKDMA(&_t_

Device

Handle, hdmarx, _t_

Device

RxDmaStreamHandle);

// defining memory address, size...etc

HAL_UART_Receive_DMA(&_t_

Device

Handle, __au8_StorageBuffer, __u16_MaxDataLength);

I checked the DMA register and they seemed correct :

CCR3->EN  = 1 // channel is enabled

CCR3->TCIE = 1 // transfert complete interrupt  is enabled

CCR3->TEIE = 1 // error interrupt enabled

CCR3->DIR = 0 // from peripheral to memory

CPAR3 has the UART RDR address

CMAR3 has the Rx buffer address.

I'm not sure what I missed here. Any suggesting on how I can debug this further ?

Thank you

regards

#dma #stm32l4 #hal #uart
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on March 29, 2018 at 10:58

Looking at Cube's sources it appears you are supposed to fill the required setting of CSELR into .Request field of the init struct.

JW

View solution in original post

7 REPLIES 7
Tilen MAJERLE
ST Employee
Posted on March 27, 2018 at 13:38

Hello

c.malki

‌

which channel and stream setup do you use?

Best regards,

Tilen

Hicham Chaabane
Associate III
Posted on March 27, 2018 at 14:02

Hi Tilen,

Sorry I forget to mention that.

I use 

DMA1_Channel3 for Rx and DMA1_Channel2 for Tx. and STM32L475

I added them in my post

Posted on March 27, 2018 at 23:34

And the respective field in DMA_CSELR is set properly?

JW

Posted on March 29, 2018 at 10:38

The CSELR register is set to 0 which is not good !

Based on the manual, the bits 11:8 should be set to 0010 to map the DMA to USART3_RX.

I'm trying to figure it out but the only place where the DMA_CSELR is set is in the HAL_DMA_Init()

/* Reset request selection for DMA1 Channelx */

DMA1_CSELR->CSELR &= ~(DMA_CSELR_C1S << hdma->ChannelIndex);

/* Configure request selection for DMA1 Channelx */

DMA1_CSELR->CSELR |= (uint32_t) (hdma->Init.Request << (hdma->ChannelIndex));

looking into this function, it seems that that both variables Init.Request and hdma->ChannelIndex are set inside the DMA init function aswell !

Any idea how to set this properly ?

Thx

Posted on March 29, 2018 at 10:53

I don't use Cube so I have no idea, sorry.

JW

Posted on March 29, 2018 at 10:58

Looking at Cube's sources it appears you are supposed to fill the required setting of CSELR into .Request field of the init struct.

JW

Posted on April 04, 2018 at 09:47

Indeed, I missed this configuration

Thank you for the help