SPI issues with the W5500 and STM32G474RE can often be traced to configuration mismatches or hardware problems. Make sure the SPI peripheral is correctly initialized in your STM32 firmware, and confirm that the W5500 is powered properly. Additionally...
It sounds like you're encountering an SPI communication issue between the W5500 and STM32G474RE. First, ensure that the SPI clock speed is within the W5500's supported range (typically up to 80 MHz). Double-check the SPI mode (CPOL and CPHA) to match...
<p>Changing the period and pulse width in HRTIM for SimplePWM requires careful handling of the timer settings. You can update the <code>PERx</code> register for the period and the <code>CMPx</code> register for the duty cycle. If you’re using STM32Cu...
<p>To change the period or pulse of an HRTIM-based SimplePWM, you’ll need to modify the relevant timer registers in your STM32 firmware. Specifically, you can adjust the <code>PERx</code> register to change the period and the <code>CMPx</code> regist...