For Non mesh beacon, BluenrgMesh_CustomBeaconReceivedCallback will be used. Its need to modified as per the use . One can add filter that only to print those data which are being advertised from social distancing sdk , like as per the log of Social ...
Hi,BluenrgMesh_CustomBeaconReceivedCallback api is used to retrieve Non mesh beacons .Since there can be numerous non mesh beacons from nearby , so kindly apply filters to retrieve iBeacon data only in BluenrgMesh_CustomBeaconReceivedCallback api, a...
Hi ,Couple of query from my side, which board is being used for social distancing Why mesh node is require to retrieve the beacon data, it can be also done using the social distancing sdk as in social distancing SDK . the device works as scanner as w...
Hello,So couple of points i would like ask for understanding the situation betterWhat is Current Stack in BlueNRG-MS module?Which firmware is being used ?Is there any resistance to reset?Are you able to pass any generic API of HCI layer like hci_le _...
Hi,Try to crosscheck the SPI I/O for sensortile (major issue)Use the HCI layer as provided in X-CUBE-BLEMESH1Also can you please Increase some delay (400 ms ) after setting RESET pin of spi in BlueNRG_RST (stm32_bluenrg_ble.c)and use the BlueNRG_RS...