I think the issue comes from the RDP value in OPTR register. The minimum RDP value that can be set for a SFI is 0.5 (0x55) because the goal of the SFI procedure is to protect the user's firmware from the contract manufacturer.After a SFI procedure, t...
Hello,It seems like the error occurs while processing the second area which contains the Option Bytes to set.The Option Bytes template file for U5-2M RSSe SFI v4.0.0 is as below:OPTR,0x9DA9F955NSBOOTADD0R,0x0800007FNSBOOTADD1R,0x0BF9007FSECBOOTADD0R,...