Originally posted as a comment on the How to write your question to maximize your chances to find a solution article.Moved to the forum for clarification & better discussion.How to create programming code based on the information ?
Input pin 2 is crankshaft position sensor counting pulses. Input pin 3 is reference sensor to toggle LED1 at pulse 20 to go LED1 high at pulse 17 till 20.3) Output pin 9 is LED14) Output pin 10 is LED2 At start up the engine both LEDs go HIGH every h...
Merged from separate thread.I would like to ask if this device can read input digital and analog signals 5 volts and output 5 volts on and off in milliseconds STM32F412G-DISCO. Who can help create programming code based on information ?Discovery Deve...