User Activity

In the case where USB power is first applied and a 20V contract established, the STUSB4500 would enable the power path to Vsnk as per usual. Then assume a 20.9V (for example) secondary power source is applied to the Vsnk output (say from a wall adapt...
Posted on April 27, 2018 at 23:51 STM32F407VETxBlank CubeMX project template plus USB_DEVICE middleware using CDC classSW4STM32firmware STM32Cube FW_F4 V1.16.0only modified code from generated templates is this (in main.c):  /* USER CODE BEGIN 2 */...
Posted on August 01, 2016 at 16:02 Overall objective: Using https://github.com/groupgets/purethermal1-firmware as a base, add a USB serial port interface (which would replace the DEBUG functionality it has currently). I have read thro...
Posted on March 31, 2016 at 15:28I'd like to know if the STL62P3LLH6 P-channel MOSFET's Safe Operating Area chart is correct in http://www.st.com/web/en/resource/technical/document/datasheet/DM00105886.pdfhttp://www.st.com/web/en/resource/technical/...