User Activity

I am unable to obtain ADC values and would like some advice.Here is the source code project.https://github.com/katsumat/STM32CubeIDE/tree/main/workspace_1.16.1/ADCCalibration PA0 is connected to GND, PA1 to Vdd, and PA3 to the output of a variable re...
Hello,I am not receiving SPI interrupt on the NUCLEO-G491, and I would like some support.Here is the source code project.https://github.com/katsumat/STM32CubeIDE/tree/main/workspace_1.16.1/SPI Specifically, I would like to perform the following actio...
Kudos given to