Posted on October 23, 2015 at 16:13Hi John,if you send some data via uart during data mode all the stream will be transmitted as data stream via wifi. If you want to return to command mode you have to send via uart the escape sequence AT+S. in a sin...
Posted on October 19, 2015 at 10:48I Mark,I used an oscilloscope and also my RTS line seems to stay low all the time. This is very strange!I found my problem, it was an issue in the configuration of the uart of my mcu. Now it works. I also changed t...
Posted on October 16, 2015 at 16:38Hi, i'm working with spwf01 module and trying to enable hardware flow control using the AT cmd at+s.scfg=console1_hwfc,1.But when enabled the module didn't give any data on the tx line. I'm using baud rate at 11520...