Hello, The MACHINE_FEATURES affect the hardware configuration and if wifi and bluetooth are set, the firmware associated are installed. For the tools on userland, it's mainly DISTRO_FEATURES which manage to add some tools depending of features set. I...
Hello Lorenzo, As you can see on the previous log, there is a syntax error on your network file: /etc/systemd/network/wireless.networkThe section must be declared under bracket and the first letter of section must be on uppercase. For more descriptio...
Hi, The append instruction of IMAGE_INSTALL_append dos not add space on your IMAGE_INSTALL variable that means you have concatenated the existing content of IMAGE_INSTALL and 'nodejs' is why you see 'nodejsopenssh-sftp'.To solve it you need to add s...