User Activity

Hi all,I selected the L6981C50DR for my DC DC buck converter with the following external components and schematic for my application:Cin: GRT31CR61H106KE01L Multilayer Ceramic Capacitors MLCC - SMD/SMT 10 uF 50 VDC 10% 1206 X5R AEC-Q200 RoHS Complian...
Hi all, I selected the L6981C50DR for my buck DC DC power module. A quick overview of my application, I am going to use this power module to convert a typ 12.8V from a smart battery to 5V @ I_out_max= 500mA (Based on experimental values, also this va...
Kudos given to