Posted on May 17, 2011 at 12:58Hi all, Finally, I have figured out what the exact problem is, but still I don't know how to solve it, so some help would be appreciated :D In the PWM example, the Frequency and the DutyCycle are calculated in the Inte...
Posted on May 17, 2011 at 12:58Quote:1) PA1 can be placed into alternate function as Tim2_Ch2. Is this what you're doing to read/decode the PWM input signal? Yes, that's what I'm doing, I configured TIM2 CH2 to read a PWM signal. Quote:2) Have you i...
Posted on May 17, 2011 at 12:58well, this thing is getting weird... I found out that if I disconnect the signal I was PWM injecting to the PA.01 the USB works right, it's only when I put the signal when all crashes... any ideas? Thanks, Sergio [ Thi...
Posted on May 17, 2011 at 12:58Hi, I'm very new to the STM32, I have an Olimex Header Board (STM32F103RB 64pin). As I'm starting, I'm testing all the ports I will have to use for my project, that includes using a virtual COM port to communicate with...