Hello NirAlon,I know that this thread is two years old but I will share a thought you should consider. The USB full-speed clock tolerance specification of +/-0.25% is specified to guarantee a maximum cable and hub setup. Which means that the complet...
Hello Simo_Sappo,you didn't provide much information about the type of your HID project, so I can't offer a concrete way to build your project at the moment. Are you planning a project based on the standard HID class or do you want to develop a custo...