Thank you, Julian.Understood, I look forward to the development team's work.I have one more request.When running detection on the emulator, "Threshold:90" is displayed on the right side of the graph, but it hides the latest results and makes it diffi...
When I use the serial emulator, I always have to change the COM and Baudrate settings.How do I save my settings or change the default settings? PSI was able to get the rock-paper-scissors detection to work on the STM32H7.
Hello Julian.By turning off the PC's WiFi, I was able to check the operation in the previous development environment.(The previous version was V4.4.0.) And I was able to use the emulator & experiment with V4.6.0.I was able to confirm the operation of...
Thank you, Julian.I was able to find the Emulator. And enter the previously used test data from the serial.Also, input the test data file from experiment. One more question.Can I use V4.3.1 without updating to see what I've worked on before?When I us...