User Activity

I am designing a PV cell charging circuit with SPV1050.When the configuration is set to boost mode, I am curious what happens if a voltage higher than Veoc is applied to the PV cell.
If you look at the SPV1050 constraints item in 6.4 MPPT Setting in the SPV1050 Datasheet, it is clearly stated that Vmpp(max) should not be applied over 2.1V.However, looking at an4397 (Application Note), even if Vin (Range: 2.6V ~ 9V) is more than 5...