User Activity

Posted on May 18, 2017 at 17:51Hi all,In my application I am using M24SR02 where the same part of the chip is being read through NFC and I2C interface at the same time. NFC reader is working in infinite loop and does two things:1) Reads 0x10 bytes f...
Posted on May 18, 2017 at 11:28Hi all,In my application I am talking to M24SR02 chip over I2C with 100kHz clock. The problem I am having is with ReadBinary command. In the application I issue exactly the same ReadBinary command over and over again -...
Posted on September 28, 2015 at 23:53Hi all,I am using STM32F030R8 MCU with STM HAL libraries. My application is running from Flash and I would like to use last page of the Flash to store some parameters. At some point the application will erase tha...