User Activity

Hello everyone,I am looking for middleware to control NAND flash using the STM32U535CE.The target device is the Macronix MX35LF4G24AD.I would like to perform page program/read, bad block management, and 8-bit ECC processing per 524 bytes. However, I ...
Hello there, We are designing the STM32U535 to operate in a low-power configuration. According to the datasheet, the current consumption in Run mode is 16.3 μA/MHz at 3.3 V, which is quite low. However, when measuring the actual device, even after su...
Hello,I am using STM32U535CEU6 for my development.I would like to transition to the bootloader using USB DFU with Boot0 pin kept Low, and the control performed within the application. I executed the following code right after HAL_Init();, but when I ...
Kudos given to