Hello @mobaid I am using the evaluation kit from ST :It’s been super useful since it can trace TOBJECT, TPRESENCE, and other values in real-time. It really helps to understand why sometimes we get detected and sometimes not, like in this situation :B...
Hey @mobaid,When I ran some detection tests without a lens, I found a FOV of about 97° (+/- 48.5°), but it wasn’t uniform at all. Also, I remember using a really low threshold (around 50 or 70), but after reading other threads, it seems like no one u...
Hello, according to this conversation, your problem was that 'A cold object inside of the FOV exits'. But I don't understand why ..Moreover, why selecting absolute value of TPRESENCE would solve detection issues ?
Hello,According to this document https://www.fresnelfactory.com/fresnel_list/en_poly_materialofFresnel.pdf, it seems that the transmittance is 42.81% (because the material of the lens is Poly FIR 200) but I also would like to be sure if I am not wron...
Hello,I've encountered a similar issue with my IR sensor setup. In my use case, I need to ensure that the power consumption stays below 10 µA.Through my research, I’ve learned that for detecting a person within a field of view, the low-pass filter cu...