Posted on January 24, 2018 at 03:15Can_TX is showing no activity. I can't figure out what I am doing wrong. I've set up the project with STMCubeMX to use CAN1 on PD0 and PD1. When I attempt to transmit there is no signs of life on the TX pin. Using ...
Posted on July 02, 2015 at 20:50
Hi,
I currently have an issue with TIM1 being reset unintentionally by the relationship between TIM2 and TIM5. My system has TIM2 encoder counting and generating a TRGO during compare pulses. TIM5 is set i...
Posted on January 25, 2018 at 18:52Ah ok that makes sense then. I ended up getting it working last night after many attempts. Two notes from my headaches :1) I was using the wrong clock speed when calculating the settings for the CAN bus, it was con...
Posted on January 25, 2018 at 03:36I went from STM32Cube_FW_F4_V1.18.0 to STM32Cube_FW_F4_V1.19.0 and I'm having a little more luck. TX and RX just spit identical garbage data when I try to transmit though. I'm not 100% sure what that is about. http...