Posted on July 06, 2015 at 12:20For problem 1. it may not caused by DfuSe Demo tool. Can anyone advise why the dfu files have different behavior ?? anyone can advise what's wrong with my procedures ?? '' 1. Downloaded the .dfu file of Mass Storage d...
Posted on July 06, 2015 at 11:30 i solved the problem by changing thestart addressof flash to 0x8003000 from 0x8000000 on step 3. and i canconvert and download the rebuilt firmware successfully. But, i have two new problems. 1. Downloaded...
Posted on July 06, 2015 at 05:15 Hello, anyone help me! i would like to generate a dfu file for STM3210B-EVAL board, but i met the following error when using DfuSeDemo.exe (3.0.0) to download firmware into the board. (As there is bug to create im...