Hello,The NEW STM32L4P5xx/L4Q5xx devices comes to complete the STM32L4+ Series portfolio.The new STM32L4+ offers a large package offer from 48 to 169-pin packages with several options.- The STM32L4P5 with 512 Kbytes to 1 Mbytes of Flash memor...
Hello @LLr.1 As stated by Richard normally you should not need to install the driver on Windows10.What I recommend is to make sure to upgrade the firmware on your X-NUCLEO01A to the latest available version (actually v1.0.8), once done you should no...
Thank you Andreas for your feedback !I agree with you about the misleading dummy cycles, and this will be fixed in future Reference Manual revisions.I recommend to take a look to the latest OCTOSPI App Note describing the new OctoSPI features: like ...
Hi Andreas,The STM32L4P5/L4Q5 and STM32H7B3/H7A3 have a new OctoSPI controller version which is working well.Can you please state which are the issues you are facing? Do you interfacing an external Octal FLASH, PSRAM or other... ?Thanks !
It seems I missed one point in your initial post, the SSD1963Yes, if you want to use the L4+ for that display you should use the SSD1963 + FSMC peripheral (8080), but here the display will be controlled by the SSD1963 NOT the internal LCD-TFT (LTDC)....