User Activity

 We want to use iio buffers to read accelerometer data. I tried the following, but it did not work. root@FAFUSION:/sys/bus/iio/devices/iio:device2# ls buffer current_timestamp_clock events in_accel_scale_available in_accel_y_raw mount_matrix of_...
We are using the X-STM32MP-GNSS2 (with the STM32 discovery board DK2), which has ISM330DHCX IMU. The accelerometer readings seem fine from the IMU, but the gyroscope gives enormously high and varying readings even when we are stationary. See below th...
Hello, Does ISM330DHCX support Dead Reckoning like ASM330LHH?If yes, can we load the Dead reckoning firmware on X-STM32MP-GNSS2 with the ISM330DHCX module?
Hello,Does ST Micro provide a Dead-reckoning GNSS expansion board/module supporting IRNSS (L-5 band NAVIC constellation)?Does X-STM32MP-GNSS2 with LIV4F eval board support TESEO-DRAW?
Hello, We are evaluating the X-STM32MP-GNSS1 eval board on STM32MP-157F-DK2.The X-STM32MP-GNSS1 has Teseo-LIV3F GPS receiver on it, which does not support NAVIC.Since we want to test receiving signals from NAVIC specifically, can we replace the Teseo...