Hello EDust, Better late than never but it could help other people. A possibility is that the edges of SCL and SDA are too steep. A possible solution is to add resistors on SDA and SCT to reduce the edges. Gaël
Hello ImegurasEs, The TSC1641 has only 4 possible I2C addresses. To use 6 devices you need to use 2 different I2C buses.In I3C, it is possible to use 6 different devices on the same bus thanks to the use of dynamic addresses. You have to follow th...