User Activity

I am using STM32H747BITx MCU and i've try CubeMX6.12.0 ,CubeMX6.10.0.Still the same problem. If I do not enable TouchGFX in CubeMX, I can successfully generate the code. However, if I enable TouchGFX, an error message like the one shown in the pictur...
I'm using RVT101HVSNWC00-B.I use TouchGFX 4.24.0 to generate initial code. There's no MX_USART2_UART_Init(); , even though I generate code again through CubeMX. I have to add it by myself to initial USART2.  
Hi,I am using the TouchGFX video widget to play custom videos on the STM32H747I-DISCO development board. I am able to play videos by placing them in the assets/videos folder and modifying Screen1View.cpp as described in the MJPEG Video . The video pl...
Kudos given to