User Activity

Hi,I am using DMA1 stream 3 for USART3 for tx on an stm32f429.Driver code is based on cubemx generated st hal drivers firmware package version 1.24 The uart and dma initalisation parameters are as follows:huart3.Instance = USART3;huart3.Init.BaudRate...
For some reason in the dialog box that appears when pressing control+H I cannot enter (or copy paste) search strings anymore than contain spaces, or ', or ", etc...[azAZ09:\] still work (and probably a few others, i did not test them allIs there some...
I just installed en.stm32cubeprg-win64_v2-7-0.zip.Installation went without problems but when I try to start the application I get the splash screen and then it just exits apparently. If I runt it from a prompt I get no messages.C:\Program Files\STMi...
After connecting a STN32H735G-DK board to my windows 7 pro pc, the com port driver gives an error "Windows cannot verify the digital signature for the drivers required for this device. A recent hardware or software change might have installed a file ...
Hi, I would prefer to use my segger jlink debugger with the discovery board io using stlink. I see there is an unpopulated header with 3V3 , SWCLK, GND, SWDIO on the left side of the board, and there is an NRST pin on the back connectors so I think ...
Kudos from