hello,It seems you are using an older version of this SSD (Standard Software Driver). Could you please download the new one (SPC58xEC-FLASH-0.2.2) and let me know? At the moment this new version is available only on TeamSpaces.I confirm also the max ...
Hello Yannek,....some answersThe same sections of RM say:"The LOCK field is not writable:– Once an Interlock Write is completed until MCR.DONE is set." I observe, that write to LOCKx registers (restoring the lock) is not possible right after MCR.DONE...
Hello Yannek,please find below some answer for your questionsI found some incosistencies between Reference Manual RM0403 and actual behaviour of SPC582B50 flash registers.According to RM section 32.3.2.3 to 6 - all LOCKx registers should be set to al...