Posted on October 18, 2016 at 08:46Increase the range doesn't change the power capability of M24LR it only change the current trigger value to start delivery , this mean if your applictaion need 3mA set the caliber to 3mA EH will be set only if 3m...
Posted on February 12, 2016 at 13:40Dear , until now NFC Forum as not yet define a T5T reference listener (Tag reference 15693) , that could be used tpo evaluate NFC poller when using Type V Technologie (ISO/IEC 15693) , but ISO as done it (ISO/...
Posted on November 26, 2015 at 17:02 The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&id...
Posted on November 18, 2015 at 09:46Dear, if your command PWD_Auth is correct and if your tag responds , (you can check it with a scope and a loop to spy the communication) , CR95HF probably miss the reply because it is out of Max frame delay time ...
Posted on November 17, 2015 at 15:46Hello , basic sequence is 1) present valid I2C password 2) protect zone by writing correspondant I2C write lock bit this protection will be activated on only after presenting a bad password or after a POR , 3) e...