Hi all,I'm using a F103 on my current project. I have trouble using the PA15 as TIM2_CH1 which is connect to a LED. I also have a serial flash connected via SPI on PB3 to PB5. As long as I don't activate the corresponding SPI timer in the RCC_APB1ENR...