User Activity

Hello,Looking at the documentation of the M2SA module, I noticed that the function of the same pins (21, 22, and 23) differs between the datasheet and the application note. Does anyone know the exact function of these pins? M2SA - application noteM2S...
In the datasheet of the BLUNERG-M2 module, it states the following:"The BlueNRG-M2 module allows applications to meet the tight advisable peak current requirements imposed withthe use of standard coin cell batteries. Optimized results are obtained wh...