Posted on April 15, 2015 at 20:34
Hi, I have a problem with interrupt of WakeUp Timer.
Never set flag for WakeUp interrupt. WakeUp timer is on EXTI EXTI of interrupt is set for rising edge and and line
Can you help me?
Thanks a lo...
Posted on April 18, 2015 at 00:27It works :-)''In addition, the RTC keeps on running under system reset if the reset source is differentfrom the power-on reset one. When a power-on reset occurs, the RTC is stopped and all theRTC registers are set to...
Posted on April 16, 2015 at 15:26New info. If I load code to the STM32L100, the uP doesn't work. But, If I connect STM32L100 discovery to the USB, the uP works! And when I press reset, the uP doesn't work again ... :-/