Hello Josh It is not possible to understand from the information what is happening, but I would try to decrease the current in the motor to understand if the measurements become identical again by changing the direction of the motor itself. This is b...
Posted on October 22, 2015 at 17:05Ciao JMwhat you mean with ''configure a RTC'': do you want to provide a 32 kHz signal externally to the BlueNRG?RegardsDino
Posted on May 14, 2015 at 11:51The inductor is used to reduce the coupling between the RF signal and the high frequency crystal that is high in some BTLE channels. Its valu depends from the layout of the board, a good starting value can be 3.9 nH