User Activity

Hi I cant seam to get the F7 to transmit the TDM output in the correct timingI have SAI Block A1 as the Slave Mode RX and B1 as the SAI TDM Tx that is sync to Block A1The Format is 8 x 32Bit Slots TDM Slave mode to a DSP Via DMA Circular bufferWhat ...
Posted on May 10, 2015 at 08:48Hi All I want to use the F429 as a USB soundcard  for a windows pc. with Both Inputs (Mic) and outputs(speaker) Only need 16khz 16bit sample rates. I cannot appear to find  any ST reference designs I have heard about t...
Posted on April 04, 2015 at 05:07Hi I want to save a Flag during a reboot on STM32F429IAt Main()I have  uint32_t bt; HAL_Init();  /* Configure the system clock to 180 Mhz */   SystemClock_Config();    __PWR_CLK_ENABLE();   HAL_PWR_EnableBkUpAccess...
Posted on March 31, 2015 at 17:57Hi I am trying to jump to the bootloader  on F429z  with using B0 B1 pinsusing the code belowbut when i send 0x7f on uart1 (from my remote client app) I get no response back at allI have confirmed Buad rate 57600 8e1...