Posted on March 05, 2015 at 09:44Hi Mr Clive1Tanks of your answerI have used all of the I/O pins for ADC,DAC,PWM IN,PWM OUT, Graphical LCD ILI9325, Keyboard ,Quadrature Encoder, &... .I want control this system with the lowest interrupt and most ex...
Posted on March 04, 2015 at 20:34 Hi Mr. Clive1 tanks of your answer. I want config ADC1&2 in dual mode with TIM4_CC4 Trig and Read result in ADC1_EOC. but it dont work. I copy my code here please help me about it. I use STM32F103 tanks ...
Posted on February 21, 2015 at 18:14hi Mr. clive1tanks of help you for ourI use stm32f103 serise mcuI want config adc1&2 in dual mode with tim4_cc triger mode without use an external pin.I want confirm it such as internal event. because i use all I/...