Posted on May 17, 2011 at 13:12Hi Andy, Thankyou for your help. This works well for me too. have implemented and tested it and all seems well. Cheers, Gareth
Posted on May 17, 2011 at 13:12Hi all, I have two programs stored in flash memory and whish to be able to switch between the two. I have a known address for each that i wish to switch too and hence would normaly use inline assembler to create a Bran...
Posted on May 17, 2011 at 13:12I have tried this method with little/no success. is it possible to do it using embedded assembly? if so can some one please show me an example.
Posted on May 17, 2011 at 13:12I got around this by adding a different programming algorithm (STM32F10x Flash Options) to the target options. (this is in uVision) Their seems to be a different algorhthm for the flash options bytes, adding this, toge...
Posted on May 17, 2011 at 12:51Hi all, sorry for the very late reply on this topic. I finaly found a solution/the problem a few weeks back. It seems that on the MCBSTM32E eval board not all the GPIO pins are physicaly connected to their labelled pad...