Will be looking for a simple sequence to activate the Outputs of the L9026 Note:- INT0 and INT1 are used to activate the chipQuick Response will be greatly appreciated.Thanks,Krishna
Recently started working on the L9026 Device, as an initial setup, trying to read the Device ID.
With The L9026 Evaluation board Device ID is read as 0x55,
With L9026 Placed on the Our Target Board, Device ID is read as 0x56,
Was surprised with t...
Hi Peter,Thanks for the quick reply. on the EVAL boards i can see BB label on L9026 Chip, i don't see any label on L9026 Chip on the Actual Target Board.Eval boards are purchased here in the USA, while our target boards are manufactured in India, Doe...