Hello,1) you need to keep the default values in the antenna parameter section, because it wants to calculate the tuning caps for an antenna that is not yet matched to 50Ohms. So, you need some values to calculate the left part of the cable.2) the pur...
Hello,the appnote AN5592 already describes which component values to use for a single ended configuration with STEVAL antenna. You would need to additionally disconnect the second antenna damping resistor and ground this antenna end. Then switch to o...
Hello,the FXR.01.07.0100C.A is an already matched 50Ohm antenna. If you intend to use this antenna, you need to select the single-ended-cable configuration in the drop down menu of the antenna matching tool. Since the antenna is already 50Ohm, you do...
Hello,you can use the St25R3916Disco for testing, but you would need to set bit d_res<3:0> in TX driver register to 2 in order to emulate the ST25R3918 driver capability. Furthermore, you need to ensure not to exceed a maximum driver current of 85mA ...
Hello,please have a look at this link:https://www.st.com/content/st_com/en/products/nfc/st25-nfc-rfid-tags-readers/st25-dynamic-nfc-tags.htmlBye,Carlo