Hi @MKana.1 ,This build issue occurs if you're compiling the kernel with CONFIG_DWC2_HOST.Normally, if you apply OpenSTLinux fragments (also available here: https://github.com/STMicroelectronics/meta-st-stm32mp/tree/thud/recipes-kernel/linux/linux-s...
STUSB1600 Linux driver is being written. For the moment, it is really basic and allows to configure STUSB1600 (power role, power operation mode). And Type-C connector is forced to Peripheral role on DK, Host role use cases can be done with Type-A con...