Posted on April 08, 2016 at 17:47Dear TwisterSIM user, the tool includes a library of M05E models for truck applications (@24V), a library of M05 device models for motor control and the new M07 devices (@ 12V). These latter ones cover all the previ...
Posted on February 04, 2015 at 12:48It is always possible to create directly inside the tool the custom Vbatt profile (Values vs Time). Please see the related Vbatt Help section in case of doubts. Best Regards
Posted on January 28, 2015 at 12:07 Hi, enclosed two examples regarding the VN7016AJ and VND7140AJ HSD devices. In the .zip files both the layout and the output signals for each device are included.
________________
Attachments : V...