Posted on March 13, 2015 at 13:17play mp3 with USB via DMA , then UART interrupt Handler miss some data sir, i am working on a project in which we use stm32f407 discovery board, in which we play audio song with USB using DMA (DMA1 stream7) , a...
Posted on March 14, 2015 at 06:21 play mp3 with USB via DMA , then UART interrupt Handler miss some data sir, i am working on a project in which we use stm32f407 discovery board, in which we play audio song with USB using DMA (DMA1 ...
Posted on January 17, 2015 at 11:51Flash Loader Demonstration error on (stm32f407 discovery board) sir i used PB10 and PB11 as serial communication(USART 3) and connect BOOT 0 pin with VDD and PB2(boot 1) to GND. But its not working and there is ...