Hello,If JCOMP is floating and debugger is not connected, this bit is used to enable host based debugging. By default when debugger is not connected (and JCOMP is floating or connected to GND), debug and trace logic remains in reset. Setting this bit...
Hello, It could be to MPU configuration. I suggest to put code in EL2 after MPU configuration for. I don't think the code can brick the device. ST Restricted
What is the JCOMP configuration of the DAP connector? As the debugger is not connected, is it floating? Or do you force this pin to 1. If you don't use any hardware configuration, can you try to set a logic value 1 on JCOMP pin?