I think it is something to do with STLinkUpgrade tool v3.14.5 which is part of Cube32 IDE 1.15.0.I got my debugger to work by reverting CubeProgrammer v2-16-0 to v2-15-0. CubeProgrammer v2-15-0 comes with STLinkUpgrade tool v3.13.4. Although not the ...
1. Why does it require the target VDD to be connected to update st-link firmware? Isn't it powered by the USB host bus? The target does not expose VDD. We only use SWDIO,SWDCLK and GND.3. The log above is when I click connect. It shows no error. So I...
I have been using CubeIde 1.10.0. But as part of project migration had to upgrade to 1.15.0. But the ide wont download the application image till I upgrade the firmware of StLink. Unfortunately, stuck with the STLink firmware upgrade!
I am getting the same error on a genuine ST Link v2. My StLink looks like https://uk.farnell.com/stmicroelectronics/st-link-v2/icd-programmer-for-stm8-stm32/dp/1892523