User Activity

I'm using the ST Visual Developer V4.3.12 and trying to do what sample stm8s code suggests, namely set a breakpoint on TRAP interrupt (which I am 99% sure it tripping because of a bug in my code).  The debugger keeps "moving", i.e. removing the break...
How do I correct this code so that the pointer is a constant and not place into RAM?```const typeOfVariable Variable = DEFINED_VARIABLE_VALUE;const typeOfVariable *pVariable = &Variable;````pVariable` keeps ending up in RAM and I've run out of ideas ...
I am using the STM8S bootloader via a USB/FTDI.  I can use Wireshark/USBpcap and catch the exchanges and I have a somewhat happy "export packets, parse with Python" method of looking at the exchange.But has anyone already written a proper Wireshark d...
I have followed AN2959 and have a bootloader running on an STM8S Discovery board but I cannot make either the command line or GUI based STMFlashLoader programs upload a program - can anyone help?- The command line version always says `No response fro...
I have seen a number of questions about reading the stm8s mapfiles and I was also someone who struggled so the attached tool might be helpful (and do let me know of any errors!).The key elements are:- There are some elements that are stored in ROM ("...
Kudos from
Kudos given to