Theng
Associate II
since
2024-03-02
2024-03-09
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About Theng
Options
Report User
User Activity
Posts
Replies
X-Nucleo-IHM07M1 Voltage
2024-03-09
I have the X-Nucleo-IHM07M1 siting on top of NUCLEO-F302R8 as shown attached. Trying to connect as follow? It is possible to connect 24V onto this board to drive 24V 3 phase motor?
X-NUCLEO-IHM07M1 Voltage
2024-03-02
Can J1 apply with 24V so 24V motor can be used on J2?
Re: X-NUCLEO-IHM07M1 Voltage
2024-03-03
I have the X-Nucleo-IHM07M1 siting on top of NUCLEO-F302R8 as shown attached. Trying to connect as follow?
Re: X-NUCLEO-IHM07M1 Voltage
2024-03-03
I have the X-Nucleo-IHM07M1 siting on top of NUCLEO-F302R8 as shown attached