User Activity

Hello,I am using the STM32H743ZI2 controller with Cortex-M7 and firmware version 1.11.2 for a project where I am capturing camera data through DCMI and sending it over Ethernet using UDP to software that receives the data and builds a video stream.Ho...
im using stm32h743zi2 nucleo board . im triyng to do programming in ethernet with udp without freeRTOS . using firmware version of 1.10.0 but it is not pinging .  anybody  did programming with this FW  . please let me know the reasons for not ping.or...
i was tried with cubemx 5.4 and fw 1.5.0 ethernet ping is successfully done. but now im trying to ping with cubemx 6.11.1 and FW 1.10.0 but im not able ping . so anybody done with cubemx 6.1.0 and above version. plzz help me on this.... thanks,,,,,,,...
I am using stm32h743 mcu and initialized cdc usb fs with cube mx for device only. After that i changed  descriptors of cdc with uvc descriptors now the device is recognized as usb composite device on device manager but i am not able to transmit any d...
i need a ioc file for properly pinging ethernet code with udp protocol on stm32h743 and cubemx 6.10.0 and firmware version 1.10 . thanks .....  
Kudos given to