For the SPV1050, what is the charge current to the battery? Can I set the current?Also, I would like to verify that when there is no voltage input to the SPV1050 that the two LDOs are off or not operating.
Hello Peter,So, if I am to understand correctly, the SPV1050 will charge the battery by a voltage mode, and the charge current is limited by the input impedance (switches, voltage source resistance, etc.) into the battery, and that this is not a curr...