Hello Fred,I see you have many versions for the same document why don't you use the Rev 8 of RM0433.Note that you started the thread with RM0468, related to STM32H72x/73x.Br,Jacky
Hello Fred,Thanks for a clear explanation on what is confusing. You have several questions, I will first answer to the register naming trouble.For the DMAMUX register you have two set of register one for DMAMUX1 (in D2 domain):one for DMAMUX2 (in D3 ...
Hi,I must admit that clock configuration is quite complex. For a "mechatronics systems engineer" you did not start with the most accessible device :-). If you want to dive deep into the clock configuration, why don't you have a look at the reference ...
Hello,the strategy to use low power mode can be tricky. Perhaps to find the appropriate configuration, you could use the tool provided by CubeMX: PCC. You can define a sequence of run/sleep/stop/standby and get an average current:Br,Jacky