Wow this explains a lot for me because I was sure I had u-boot working fine for a while and then it stopped working. Turns out I was compiling on another machine where I had 5.0.2 . While I had 5.0.0 on the other machine. Anyways you should update th...
HiI wonder if anyone using the standard ECO rev 5 have working U-Boot? Anyways @debugging did post a link to his discord server where the issue is described. I have added the patch that I use here in case you are not using Discord. I have to note th...
Thank you so much. It is finally working now. It seems like ST does not have much interest in having customers when they don't post these kinds of bugs publicly and that they don't make a new minor release as soon as such a bug is discovered.
Hi, I tried to post here yesterday but my post is not visible so I will try again, could be because i copied part of my boot log my have contained bad characters. So I try again. I have the exact same problem as well, it stops u-boot uart at - DDR ...
I Also have a this problem where u-boot stops at the clock 151. On thing worth to note that for me if I turn off debug printing Linux will boot just fine so u-boot must somehow run but it stops printing around the DDR frequency printing. So we are ab...